JAJSJV7C december 2020 – may 2023 TPS272C45
PRODUCTION DATA
The device monitors the supply voltage at the VS pin to prevent unpredicted behaviors in the event that the supply voltage is too low. When the supply voltage falls down to VUVLOF, the device enters the shut down state automatically. When the supply rises up to VUVLOR, the device turns back on. When the device is configured to support an external regulator connected to VDD, for proper device behavior it is required that the supply input for the external regulator is derived from the same VS supply of TPS272C45 as shown in Figure 9-6.
Fault is not indicated on the FLT pin during an UVLO event. During an initial ramp of VVS from 0 V at a ramp rate slower than 1 V/ms, VENx pins must be held low until VS is above the UVLO threshold. For best operation, ensure that VS has risen above UVLO before setting the VENx pins to high.