JAJSJV7C december 2020 – may 2023 TPS272C45
PRODUCTION DATA
All versions of the device power up from the OFF state only when the VS supply input exceeds the VVSUVLOR threshold (independent of the VDD supply input level). When VS supply is above the threshold, the internal regulators are enabled, the device version is recognized. The device then enters the standby state. With versions A, C, and D and using using an external supply on VDD pin - the device will use the internal regulators until the VDD voltage exceeds VVDD_UVLOR.
In case the VDD power supply is enabled first and the VDD voltage exceeds VVDD_UVLOR before the VS supply is up and the VS voltage exceeds VSUVLOR, the device remains in the off-state.
The behavior of all versions of the device in case of brown-out or power loss in VS supply is as described in Undervoltage Lockout on VS (UVLO). For versions A, C, and D if the VDD power supply is lost (VDD supply voltage falls below VVDD_UVLOR threshold), the device switches over to the internal power supply, the switch outputs are disabled.