JAJSLG9B March 2021 – November 2023 TPS3704-Q1
PRODUCTION DATA
Overvoltage and undervoltage comparators include built-in hysteresis that provides noise immunity and ensures stable operation. For example, if the voltage on the SENSEx pin falls below VIT-(UV) or above VIT+(OV), then RESETx/RESETx is asserted. When the voltage on the SENSEx pin is between the positive and negative threshold voltages, RESETx/RESETx deasserts after the set RESETx/RESETx delay time. Figure 7-5 shows the relation between VIT-(UV),VIT+(OV) and the hysteresis voltage (VHYS).