JAJST92A July 2017 – February 2024 TPS3710-Q1
PRODUCTION DATA
The resistor divider values and target threshold voltage can be calculated by using Equation 1 to determine VMON(UV).
where
Choose RTOTAL ( = R1 + R2) so that the current through the divider is approximately 100 times higher than the input current at the SENSE pin. The resistors can have high values to minimize current consumption as a result of low input bias current without adding significant error to the resistive divider. For details on sizing input resistors, refer to application report SLVA450, Optimizing Resistor Dividers at a Comparator Input, available for download from www.ti.com.