JAJST93A October 2015 – February 2024 TPS3710
PRODUCTION DATA
To make ensure the proper voltage level, the pullup resistor value is selected by ensuring that the pullup voltage divided by the resistor does not exceed the sink-current capability of the device. This confirmation is calculated by verifying that the pullup voltage minus the output-leakage current (Ilkg(OD)) multiplied by the resistor is greater than the desired logic-high voltage. These values are specified in the Section 5.5.
Use Equation 2 to calculate the value of the pullup resistor.