JAJSRP6A October 2023 – May 2024 TPS3762-Q1
PRODUCTION DATA
The TPS3762-Q1 comes with the optional undervoltage bypass (UVbypass) feature, check Section 5 to verify variant specific UVbypass functionality. When using a variant with UVbypass enabled, the first undervoltage event after VDD > VPOR is ignored. In cases where an undervoltage event has not occurred UVbypass can be cleared by running BIST.
UVbypass is targeted at specific applications in which the TPS3762-Q1 is powered Off-battery and is monitoring the Off-battery DC-DC output, as shown in Figure 10-7. If the Off-battery DCDC output is outside of threshold the TPS3762-Q1 resets this device. See Figure 10-8 and Figure 10-9 for more details.