The following method to design converter
compensation optimizes the load transient response.
- Calculate the require output impedance to meet
transient response goals. This equation assumes the load step transient is faster than the
BW of the converter.
Equation 9.
- Select a value for output
inductance.
Equation 10.
- Calculate the required converter output impedance
to meet the transient response goal.
Equation 11.
Make sure ZOUT_CONVERTER is less than the
ZOUT_REQUIRED found in step 1. Also recheck that the voltage on
CRAMP is within acceptable limits. (see previous section) If the voltage on
CRAMP is too large, use a larger CRAMP value. - Calculate the minimum output capacitance required
to meet the impedance requirements.
Equation 12.
where
- fCO_DESIRED is the desired converter closed loop crossover frequency,
which is usually 1/8 to 1/4 of the converter switching frequency.
- Calculate the number of output capacitors
required. From the previous section, use the guidelines for ESR to select a capacitor type
and value, then use the equation here to find the number of capacitors required. Notice
that the impedance of the capacitors (ESR plus impedance of the capacitance at the
chosen crossover frequency) is used.
Equation 13.
Equation 14.
- Using one of the tools on TI.com, simulate with
the values for the design.