JAJSP25 November 2023 TPS546A24S
PRODUCTION DATA
The initial output voltage can be set by the VSEL pin at AVIN power up. As part of power-on reset (POR), the VSEL pin senses both the resistance from the VSEL pin to AGND and the divider ratio of the VSEL pin between B1V5 and AGND. These values program (29h) VOUT_SCALE_LOOP, (21h) VOUT_COMMAND, (2Bh) VOUT_MIN, and (24h) VOUT_MAX and select the appropriate settings for the internal feedback divider and precision adjustable reference voltage. After the TPS546A24S completes its POR and enables PMBus communication, these initial values can be changed through PMBus communication.
The output voltage can be programmed through PMBus and its value is related to the following registers:
The TPS546A24S defaults to the relative format for the following, but can be changed to use absolute format through the PMBus command (20h) VOUT_MODE:
Refer to the detailed description of (20h) VOUT_MODE for details.