JAJSRI4 December 2024 TPS546B26
PRODUCTION DATA
| CMD Address | 21h |
| Write Transaction: | Write Word |
| Read Transaction: | Read Word |
| Format: | ULINEAR16 per (20h) VOUT_MODE |
| NVM Back-up: | No (VBOOT_OFFSET_1) / VOUT_SCALE_LOOP |
| Updates: | on-the-fly |
The regulated output can be set by PMBus or by the result of pin-strapping on pin VSEL. When PMBus or pin-strapping is used to set the regulated voltage, the commanded output voltage in volts is determined by a combination of VOUT_COMMAND, VOUT_TRIM, VOUT_MARGIN_HIGH, VOUT_MARGIN_LOW, and OPERATION commands, as below. As stated in the description of the VOUT_MODE command, the VOUT step size is 1.953mV.
This register can be changed during soft-start or soft-stop. However, the rail will continue to ramp up/down to the original target (VBOOT) at the rate programmed into TON_RISE/TOFF_FALL. After soft-start completes (and if VOUT_COMMAND is different from the VBOOT value), the device will immediately transition from the VBOOT value to the latest written VOUT_COMMAND at the programmed VOUT_TRANSITION_RATE. Writes to VOUT_COMMAND during soft-stop will be acknowledged, however, no transition will occur and VOUT_COMMAND will get automatically updated back to VBOOT at the conclusion of soft-stop. After soft-start has completed, writes to VOUT_COMMAND are also allowed even if the output voltage is still transitioning to a previously programmed VOUT_COMMAND. The output voltage will immediately begin transitioning to the newly programmed VOUT_COMMAND at the rate specified by VOUT_TRANSITION_RATE. The device does not wait for the prior transition to complete.
Return to Supported PMBus Commands.
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| R | R | R | R/W | R/W | R/W | R/W | R/W |
| VOUT_COMMAND (High Byte) | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W |
| VOUT_COMMAND (Low Byte) | |||||||
The programmed Vout is computed as:
default*: XXX0 0000 0000 0000 (binary) (X means writes will be ignored and reads will be 0)
VOUT = (VOUT_COMMAND + VOUT_TRIM + (VOUT_MARGIN_HIGH – 1) * VOUT_COMMAND * OPERATION[5] – (1 – VOUT_MARGIN_LOW) * VOUT_COMMAND * OPERATION[4]) * VOUT_MODE
| LEGEND: R/W = Read/Write; R = Read only |
| Bit | Field | Access | Reset | Description |
|---|---|---|---|---|
| 15:13 | VOUT_COMMAND | R | 000b | Not used and always set to 0. |
| 12:0 | VOUT_COMMAND | R/W | VBOOT_OFFSET_1 (see below) | Sets the output voltage target via the PMBus interface. |
At power up, the reset value of VOUT_COMMAND is derived from VBOOT_OFFSET_1 / VOUT_SCALE_LOOP . When the rail is disabled by the mechanism programmed to ON_OFF_CONFIG or due to a fault, the value in VOUT_COMMAND is updated to VBOOT.
When the PMB_ADDR/VORST# pin is configured as a RESET# pin in SYS_CONFIG_USER1 (EN_VORST), assertion of the PMB_ADDR/VORST# pin causes the output voltage to return to the VBOOT value in VBOOT_OFFSET_1 (VBOOT_1), and causes the VOUT_COMMAND value to be updated accordingly.
Writes to VOUT_COMMAND for which the resulting value, including any offset from VOUT_TRIM, is greater than the current (24h) VOUT_MAX or less than the current (2Bh) VOUT_MIN, causes the VOUT_COMMAND to move to the value specified by (2Bh) VOUT_MIN or (24h) VOUT_MAX respectively. The VOUT_MAX_MIN warning bit is set in STATUS_VOUT, which sets the appropriate bit in STATUS_WORD, and the host is notified per the PMBus 1.3.1 Part II specification, section 10.2.
The TPS546B26 can not produce output voltages greater than 0.75V / VOUT_SCALE_LOOP. If VOUT_COMMAND is set greater than this but lower than (24h) VOUT_MAX, the TPS546B26 will not trigger a MIN/MAX warning in Section 7.45