JAJSRI4 December 2024 TPS546B26
PRODUCTION DATA
The TPS546B26 offers both internal feedback divider (discrete) and external feedback divider (continuous) output voltage setting options.
With the continuous output voltage setting method, the reference DAC default is set to 0.4V (VBOOT_1 in VBOOT_OFFSET_1) and the external resistor divider is the equivalent to VOUT_SCALE_LOOP = 1. The divider gain is now determined by the external voltage setting resistors as described in Loop Compensation.
With the discrete output voltage setting method, the output voltage is determined by two settings: VOUT_COMMAND and VOUT_SCALE_LOOP. Together, these two parameters determine the converter output voltage. VOUT_COMMAND is used to adjust the reference DAC input to the Error Amplifier and can be in the range of 0.25V to 0.75V. VOUT_SCALE_LOOP selects a voltage divider gain of 1, 0.5, 0.25, or 0.125.
When PMBus or Pin-Strapping is used to set the regulated voltage, the commanded output voltage in volts is determined by a combination of VOUT_COMMAND, VOUT_TRIM, VOUT_MARGIN_HIGH, VOUT_MARGIN_LOW, and OPERATION commands, as below. As stated in the description of the VOUT_MODE command, the VOUT step size is 1.953mV. The programmed VOUT is computed as:
VOUT = (VOUT_COMMAND + VOUT_TRIM + (VOUT_MARGIN_HIGH – 1) * VOUT_COMMAND × OPERATIONS[5] – (1–m VOUT_MARGIN_LOW) * VOUT_COMMAND × OPERATIONS[4])
The output voltage is related to:
The TPS546B26 defaults to the relative format for the following per bit 7 in VOUT_MODE:
Refer to the detailed description of VOUT_MODE for details.
The range of recommended VOUT_COMMAND values is dependent upon the configured VOUT_SCALE_LOOP. The design does not limit the VOUT_COMMAND value to be within this recommended range. The VOUT_COMMAND value is limited only by VOUT_MAX and VOUT_MIN. The VOUT LSB is 1.953mV, the minimum VOUT is 0.25V, and the maximum VOUT is 5.5V.
| VOUT_SCALE_LOOP (V/V) | VOUT Range (V) | VOUT_COMMAND Recommended Range (dec) |
|---|---|---|
| 1 | 0.244 – 0.75 | 125 – 384 |
| 0.5 | 0.244 – 1.5 | 125 – 768 |
| 0.25 | 0.488 – 3 | 250 – 1536 |
| 0.125 | 0.976 – 5.504 | 500 – 2818 |
The TPS546B26 offers a VOUT reset (VORST#) function on the PMB_ADDR/VORST# pin. If PMB_ADDR/VORST# is low and EN_VORST in SYS_CFG_USER1[2] = 1, then VOUT_COMMAND is set to VBOOT at the setting in VOUT_TRANSITION_RATE.
Figure 6-3 VOUT Reset by
VORST#