JAJSNP4A May 2023 – February 2024 TPS54KB20
PRODUCTION DATA
The device uses a zero-crossing (ZC) circuit to perform the zero inductor current detection during skip-mode operation. The ZC threshold is set to a small negative value before the low-side MOSFET is turned off, entering discontinuous conduction mode (DCM) operation. After entering DCM, the ZC threshold hysteresis increases the threshold to a small positive value. As a result, the device delivers better light-load efficiency.
When the load current increases enough such that the device exits DCM, the ZC circuit must detect 16 consecutive cycles of negative inductor current below the ZC threshold before returning to DCM. Only one cycle without ZC detection is required to exit DCM.
When the output is enabled, the ZC circuit is also enabled during the first 32 switching cycles while the device is in soft start. If the MSEL resistor value is for FCCM, ZC is disabled and the device transitions to FCCM when soft start is complete. See Adjustable Soft Start for description on soft-start completion. If there are not at least 32 switching cycles before soft start is done, such as during start-up with a high output prebias, the ZC is not disabled until the first high-side MOSFET on-time after soft-start done is complete.