JAJSQV6 February 2024 TPS54KC23
PRODUCTION DATA
For a buck converter, during the on-time of the high-side MOSFET, the switch current increases at a linear rate determined by the input voltage, output voltage, on-time, and output inductor value. During the on-time of the low-side MOSFET, the current decreases linearly. The average value of the switch current equals the load current.
The output overcurrent limit (OCL) in the device is implemented using a cycle-by-cycle valley current detect control circuit. The inductor current is monitored during the on-time of the low-side MOSFET by measuring the low-side MOSFET drain-to-source current. If the measured drain-to-source current of the low-side MOSFET is above the current limit threshold, the low-side MOSFET stays ON until the current level becomes lower than the current limit threshold. This type of behavior reduces the average output current sourced by the device.
During an overcurrent condition, the current to the load exceeds the current to the output capacitors. Thus, the output voltage tends to decrease. Eventually, when the output voltage falls below the undervoltage-protection threshold (79%), the UVP comparator detects the fall and shuts down the device after a wait time of 70µs. Depending on the part number, the device either hiccups or latches off, as described in Overvoltage and Undervoltage Protection.
Figure 6-5 shows the cycle-by-cycle valley current limit behavior as well as the wait time before the device shuts down.
If an OCL condition happens during start-up, the device still has cycle-by-cycle current limit based on low-side valley current. After soft start is finished, the UV event which is caused by the OCL event shuts down the device after a wait time of 70µs. After UV is tripped, the device hiccups as described in Overvoltage and Undervoltage Protection.
The resistor, RILIM connected from the ILIM pin to AGND sets current limit threshold. TI recommends a ±1% tolerance resistor because a worse tolerance resistor provides less accurate OCL threshold. Equation 5 calculates the RILIM for a given overcurrent limit threshold on the device. Equation 6 calculates the overcurrent limit threshold for a given RILIM value.
To protect the device from an unexpected connection to the ILIM pin, an internal fixed OCL clamp is implemented. This internal OCL clamp limits the maximum valley current on the low-side MOSFET when the ILIM pin has too small of a resistance to AGND, or is accidentally shorted to ground. TI does not recommend designing with an RILIM < 4.32kΩ.
where