JAJSQV6 February 2024 TPS54KC23
PRODUCTION DATA
An RC snubber on the SW pin can also help reduce voltage overshoot and ringing at the SW pin. For the RC snubber to be as effective as possible with the symmetrical pinout, place the RC snubber on the opposite side of the board from the IC with multiple vias in the SW node to minimize routing impedance and with a very low impedance return to the PGND pins.