JAJSO99 april 2023 TPS552892-Q1
PRODUCTION DATA
The TPS552892-Q1 outputs a voltage at the CDC pin proportional to the sensed voltage across a output current sensing resistor between the ISP pin and the ISN pin. Equation 6 shows the exact voltage at the CDC pin related to the sensed output current.
To compensate the voltage droop across a cable from the output of the USB port to its powered device, the TPS552892-Q1 can lift its output voltage in proportion to the load current by placing a resistor between the CDC pin and AGND pin.
The output voltage rises in proportion to the current sourcing from the CDC pin through the resistor at the CDC pin. It is recommended to use 100-kΩ resistance for the up resistor of the feedback resistor divider. Equation 7 shows the output voltage rise related to the sensed output current, the resistance at the CDC pin, and the up resistor of the output voltage feedback resistor divider.
where
When RFB_UP is 100 kΩ, the output voltage rise versus the sensed output current and the resistor at the CDC pin is shown in Figure 7-6.