JAJSL43A July 2014 – September 2021 TPS55340-EP
PRODUCTION DATA
The TPS55340-EP has internal slope compensation to prevent subharmonic oscillations. The sensed current slope of boost converter can be expressed as Equation 4.
Calculate the slope compensation dv/dt using Equation 5.
In a converter with current mode control, in addition to the output voltage feedback loop, take into account the inner current loop including the inductor current sampling effect and slope compensation on the small signal response, which can be modeled as seen in Equation 6.
where
Note that if Sn << Se, the converter operates in voltage mode control rather than current mode control, and Equation 6 is no longer valid.