JAJSL03C January 2021 – December 2021 TPS61094
PRODUCTION DATA
PIN | I/O(1) | DESCRIPTION | |
---|---|---|---|
NO. | NAME | ||
1 | OSEL | I | Boost output voltage selection pin. Connect a resistor between this pin and ground to select one of sixteen output voltages of Boost mode. |
2 | MODE | I | Operation mode selection pin. The MODE pin and EN pin work together to set device operation mode. See Table 7-4. |
3 | EN | I | Operation mode selection pin. The MODE pin and EN pin work together to set device operation mode. See Table 7-4. |
4 | VIN | PWR | IC power supply input |
5 | SW | PWR | The switching node pin of the converter. It is connected to the drain of the internal low-side power MOSFET and the source of the internal high-side power MOSFET. |
6 | SUP | I | Output of buck converter to sense the voltage of the supercap |
7 | PGND | PWR | Power ground |
8 | AGND | PWR | Signal ground |
9, 10 | VOUT | PWR | Output of the device |
11 | ICHG | I | Charging current selection pin. Connect a resistor between this pin and ground to select one of sixteen output currents of Buck mode. |
12 | VCHG | I | Charging voltage selection pin. Connect a resistor between this pin and ground to select one of sixteen regulation voltages of Buck mode. |