SLVSBX9A September 2014 – September 2014 TPS61291
PRODUCTION DATA.
PIN | I/O | DESCRIPTION | |
---|---|---|---|
NAME | NO. | ||
SW | 1 | I | Switch node of the converter. Connect the inductor between this pin and the input capacitor CIN. |
VOUT | 2 | O | Boost converter output. Connect the output capacitor COUT between this pin and GND close to the device. |
VIN | 3 | PWR | Input voltage supply pin for the boost converter. Connect the input capacitor CIN between this pin and GND as close as possible to the device. |
EN/BYP | 4 | I | Control pin of the device. A high level enables the boost mode operation. A low level disables the boost converter and enables bypass mode operation. EN/BYP must be actively terminated high or low. Usually, this pin is controlled by the MCU in the system. |
VSEL | 5 | I | Output voltage selection pin. The logic level of this pin is read out during startup and internally latched. Connect this pin only to GND, VOUT, or leave it floating. |
GND | 6 | PWR | Ground pin of the device. |
EXPOSED THERMAL PAD | NC | Not electrically connected to the IC, but must be soldered to achieve specified thermal performance. Connect this pad to the GND pin and use it as a central GND plane. |