SLVS977B February 2010 – July 2016 TPS61325
PRODUCTION DATA.
PIN | I/O | DESCRIPTION | |
---|---|---|---|
NAME | NO. | ||
AGND | A4 | — | Analog ground. |
AVIN | E4 | I | The input voltage pin of the device. Connect directly to the input bypass capacitor. |
BAL | A3 | O | Balancing output for dual cells super-capacitor. In steady-state operation, this output compensates for leakage current mismatch between the cells. |
GPIO/PG | D4 | I/O | This pin can be configured as a general purpose input and output pin (GPIO), an open-drain, or a push-pull output to signal when the converters output voltage is within the regulation limits (PG). The pin is configured as an open-drain power-good output by default. |
HC_SEL | B3 | I | Extended high-current mode selection input. This pin must not be left floating and must be terminated. HC_SEL = LOW: LED direct drive mode. The power stage is active and the maximum LED currents are defined as 445 mA, 890 mA, 445 mA. HC_SEL = HIGH: Energy storage mode. In flash mode, the power stage is either active with reduced current capability or disabled. The maximum LED current is defined as 1025 mA, 2050 mA, 1025 mA. |
INDLED | A1 | O | This pin provides a constant current source to drive low VF LEDs. Connect to LED anode. |
LED1 | E2 | I | LED return input. This feedback pin regulates the LED current through the internal sense resistor by regulating the voltage across it. The regulation operates with typically 400-mV (HC_SEL = L) or 400-mV (HC_SEL = H) dropout voltage. Connect to the cathode of the LEDs. |
LED2 | E1 | I | |
LED3 | E3 | I | |
PGND | D1, D2 | — | Power ground. Connect to AGND underneath IC. |
STRB0 | B4 | I | LEDx enable logic input. This pin can be used to enable and disable the high-power LEDs connected to the device. STRB0 = LOW: LEDx current regulators are turned off. STRB0 = HIGH: LED2, LED2 and LED3 current regulators are active. The LED current level (DC-light or flashlight current) is defined according to the STRB1 logic level. |
STRB1 | D3 | I | LED current level selection input. Pulling this input high disables the DC-light watchdog timer. STRB1 = LOW: Flashlight mode is enabled. STRB1 = HIGH: DC-light mode is enabled. |
SCL | B2 | I | Serial interface clock line. This pin must not be left floating and must be terminated. |
SDA | B1 | I/O | Serial interface address and data line. This pin must not be left floating and must be terminated. |
SW | C1, C2 | I/O | Inductor connection. Drain of the internal power MOSFET. Connect to the switched side of the inductor. SW is high impedance during shutdown. |
TS | C4 | I/O | NTC resistor connection. This pin can be used to monitor the LED temperature. Connect a 220-kΩ NTC resistor from the TS input to ground. In case this functionality is not desired, the TS input must be tied to AVIN or left floating. |
Tx-MASK | C3 | I | RF PA synchronization control input. |
VOUT | A2 | O | This is the output voltage pin of the converter. |