JAJSPC6 November 2023 TPS61377
PRODUCTION DATA
The TPS61377 adopts a cycle-by-cycle peak switching current limit function internally. The low-side switch is turned off as soon as the switch peak current triggers the limit threshold. The peak switching current limit can be set by a resistor from the ILIM pin to ground. The relationship between the peak current limit and the resistor is shown in Equation 3.
where
For instance, the peak switching current is 5.4 A typical if the RLIM is 16 kΩ. ILIM pin cannot be left floating or connected to VCC.