JAJSPC6 November 2023 TPS61377
PRODUCTION DATA
The output voltage is set by an external resistor divider (R1, R2 in the Figure 8-1 circuit diagram). For the best accuracy, R2 should be smaller than 500 kΩ to ensure the current flowing through R2 is at least 100 times larger than the FB pin leakage current. Changing R2 to lower value increases the immunity against noise injection. Changing R2 to higher values reduces the quiescent current to achieve higher efficiency at light load.
The value of R1 is then calculated as: