JAJSPC6 November 2023 TPS61377
PRODUCTION DATA
The TPS61377 has a dual function enable and UVLO circuit. When the input voltage at the VIN pin is above the input UVLO rising threshold of 2.8 V typical and the EN/UVLO pin is pulled above the rising threshold, the TPS61377 is enabled and starts switching. The EN/UVLO pin has an accurate UVLO voltage threshold to support programmable input under-voltage lockout with hysteresis. A hysteresis current IUVLO_HYS is sourced out of the EN/UVLO pin to provide hysteresis that prevents on/off chattering in the presence of input voltage noise. By using resistor divider as shown in Figure 7-1 , the turn on threshold can be calculated by using Equation 1.
where
The hysteresis between the UVLO turn on threshold and turn off threshold is set by the upper resistor in the EN/UVLO resistor divider and is given by Equation 2
where