JAJSLJ1B September 2015 – March 2021 TPS62748
PRODUCTION DATA
The load switch connects VOS pin to the LOAD pin and is able to support 100 mA. The on-resistance depends on the output voltage. At 1.2 V Vout the on-resistance is maximum 2.2 Ω and at 1.8 V Vout the on-resistance is maximum 1.2Ω. The load switch can be used to power a sub system. With CTRL=high the load switch is turned on. To avoid a voltage drop at the output of the buck converter the load switch has a internal softstart. With CTRL=low the load switch is turned off and the LOAD pin is internally discharged to GND by typically 30Ω. This makes sure the output of the load switch is always discharged to GND before the load switch is turned on again.