JAJSGZ1E September 2015 – October 2024 TPS65094
PRODUCTION DATA
The master initiates data transfer by generating a START condition. The START condition exists when a high-to-low transition occurs on the SDA line while SCL is high (see Figure 7-13). All I2C-compatible devices should recognize a START condition.
The master then generates the SCL
pulses and transmits the 7-bit address and the read/write direction bit R/W on the
SDA line. During all transmissions, the master ensures that data is valid. A valid
data condition requires the SDA line to be stable during the entire high period of
the clock pulse (see
Figure 7-14). All devices recognize the address sent by the master and compare it to their
internal fixed addresses. Only the slave device with a matching address generates an
acknowledge (see Figure 7-15), by pulling the SDA line low during the entire high period of the ninth SCL
cycle. Upon detecting this acknowledge, the master identifies that the communication
link with a slave has been established.
The master generates further SCL cycles to either transmit data to the slave (R/W bit = 0) or receive data from the slave (R/W bit = 1). In either case, the receiver must acknowledge the data sent by the transmitter. An acknowledge signal can either be generated by the master or by the slave, depending on which one is the receiver. Any 9-bit valid data sequences consisting of 8-bit data and 1-bit acknowledge can continue as long as necessary.
To signal the end of the data transfer, the master generates a STOP condition by pulling the SDA line from low to high while the SCL line is high (see Figure 7-13). This STOP condition releases the bus and stops the communication link with the addressed slave. All I2C-compatible devices must recognize the STOP condition. Upon the receipt of a STOP condition, all devices detect that the bus is released, and they wait for a START condition followed by a matching address.