JAJSF01I November 2011 – March 2018 TPS65217
PRODUCTION DATA.
PIN | I/O | DESCRIPTION | |
---|---|---|---|
NAME | NO. | ||
AC | 10 | I | AC-adapter input to power path. Connect this pin to an external dc supply. |
AGND | 41 | — | Analog ground (GND). Connect the AGND pin to the ground plane. |
BAT | 4, 5 | I/O | Battery charger output. Connect these pins to the battery. |
BAT_SENSE | 6 | I | Battery-voltage sense input. Connect the BAT_SENSE pin to the BAT pin directly at the battery terminal. |
BYPASS | 47 | O | Internal bias voltage (2.25 V). TI does not recommend connecting any external load to this pin. |
FB_WLED | 38 | I | Feedback pin for the WLED boost converter. This pin is also connected to the anode of the WLED strings. |
INT_LDO | 48 | O | Internal bias voltage (2.3 V). TI does not recommend connecting any external load to this pin. |
ISET1 | 35 | I | Low-level WLED current set. Connect this pin to a resistor to ground to set the WLED low-level current value. |
ISET2 | 36 | I | High-level WLED current set. Connect this pin to a resistor to ground to set the WLED high-level current value. |
ISINK1 | 34 | I | Input to the WLED current SINK1. Connect this pin to the cathode of the WLED string. Current through the SINK1 pin equals current through the ISINK2 pin. If only one WLED string is used, short the ISINK1 and ISINK2 pins together. |
ISINK2 | 33 | I | Input to the WLED current SINK2. Connect this pin to the cathode of the WLED string. Current through the SINK1 pin equals current through the ISINK2 pin. If only one WLED string is used, short the ISINK1 and ISINK2 pins together. |
L1 | 20 | O | Switch pin for DCDC1. Connect this pin to the respective inductor. |
L2 | 23 | O | Switch pin for DCDC2. Connect this pin to the respective inductor. |
L3 | 31 | O | Switch pin for DCDC3. Connect this pin to the respective inductor. |
L4 | 37 | O | Switch pin of the WLED boost converter. Connected this pin to the respective inductor. |
LDO_PGOOD | 46 | O | Power-good signal for the LDO regulator (LDO1 and LDO2 only). This pin is a push-pull output. This pin is pulled low when either the LDO1 or LDO2 regulator is out of regulation. |
LS1_IN | 39 | I | Input voltage pin for load switch 1 (LS1) or LDO3 |
LS1_OUT | 40 | O | Output voltage pin for load switch 1 (LS1) or LDO3 |
LS2_IN | 42 | I | Input voltage pin for load switch 2 (LS2) or LDO4 |
LS2_OUT | 43 | O | Output voltage pin for load switch 2 (LS2) or LDO4 |
MUX_IN | 14 | O | Input to analog multiplexer |
MUX_OUT | 16 | O | Output pin of analog multiplexer |
NC | 15, 17 | Not used | |
nINT | 45 | O | Interrupt output. This pin is an active-low, open-drain output. This pin is pulled low if an interrupt bit is set. The output goes high after the bit causing the interrupt in the INT register is read. The interrupt sources can be masked in the INT register, such that no interrupt is generated when the corresponding interrupt bit is set. |
nRESET | 44 | I | Reset pin. This pin is an active-low input. Pulling this pin low causes the PMIC to shut down. When this pin returns to a high voltage level, the PMIC powers up in its default state after a 1-s delay. |
nWAKEUP | 13 | O | Signal to the host to indicate a power-on event. This pin is an active-low, open-drain output. |
PB_IN | 25 | I | Push-button monitor input. This pin is typically connected to a momentary switch to ground. This pin is an active-low input. |
PGND | 30 | Power ground. Connect this pin to the ground plane. | |
PGOOD | 26 | O | Power-good output. This pin is a push-pull output. This pin is pulled low when any of the power rails are out of regulation. |
PWR_EN | 9 | I | Enable input for the DCDC1, DCDC2, and DCDC3 converters, and the LDO1, LDO2, LDO3, and LDO4 regulators. Pull this pin high to start the power-up sequence. |
SCL | 28 | I | Clock input for the I2C interface |
SDA | 27 | I/O | Data line for the I2C interface |
SYS | 7, 8 | O | System voltage pin and output of the power path. All voltage regulators are typically powered from this output. |
TS | 11 | I | Temperature sense input. Connect this pin to the NTC thermistor to sense the battery temperature. This pin works with 10-kΩ and 100-kΩ thermistors. For more information, see the Battery-Pack Temperature Monitoring section. |
USB | 12 | I | USB voltage input to power path. Connect this pin to an external voltage from a USB port. |
VDCDC1 | 19 | I | DCDC1 output and feedback voltage-sense input |
VDCDC2 | 24 | I | DCDC2 output and feedback voltage-sense input |
VDCDC3 | 29 | I | DCDC3 output and feedback voltage-sense input |
VINLDO | 2 | I | Input voltage for LDO1 and LDO2 |
VIN_DCDC1 | 21 | I | Input voltage for DCDC1. This pin must be connected to the SYS pin. |
VIN_DCDC2 | 22 | I | Input voltage for DCDC2. This pin must be connected to the SYS pin. |
VIN_DCDC3 | 32 | I | Input voltage for DCDC3. This pin must be connected to the SYS pin. |
VIO | 18 | I | Output-high supply for output buffers |
VLDO1 | 3 | O | Output voltage of LDO1 |
VLDO2 | 1 | O | Output voltage of LDO2 |
Thermal pad | — | Power-ground connection for the PMIC. Connect the thermal pad to the ground plane. |