JAJSI26A November 2019 – February 2021 TPS6521815
PRODUCTION DATA
The GPIO3 is an edge-sensitive reset input to the PMIC, when the DC12_RST bit set to 1. The reset signal affects DCDC1 and DCDC2 only, so that only those two registers are reset to the power-up default whenever GPIO3 input transitions from high to low, while all other registers maintain their current values. DCDC1 and DCDC2 transition back to the default value following the SLEW settings, and are not power cycled. This function recovers the processor from reset events while in low-power mode.
Figure 8-23 I/O Pin Logic
Figure 8-24 DDR3 Reset Timing DiagramGPIO must be configured as input (IO1_SEL = 1b). GPO2 is automatically configured as output.