SLVSAE1B October 2010 – September 2015 TPS65708
PRODUCTION DATA.
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
The TPS65708 device is designed for use as a power supply for embedded camera module or other portable low-power equipment.
For this design example, use the parameters listed in Table 2 as the input parameters.
DESIGN PARAMETER | VALUE |
---|---|
Input Supply Voltage | 3.6 V to 6 V |
Switching Frequency | 2.25 MHz |
Output Filter Corner Frequency | 40 kHz |
The converter operates typically with a 1.5-µH or 2.2-µH output inductor. The selected inductor has to be rated for its DC resistance and saturation current. The DC resistance of the inductance will influence directly the efficiency of the converter. Therefore an inductor with lowest DC resistance should be selected for highest efficiency.
Equation 2 calculates the maximum inductor current under static load conditions. The saturation current of the inductor should be rated higher than the maximum inductor current as calculated with Equation 2. This is recommended because during heavy load transient the inductor current will rise above the calculated value.
where
The highest inductor current will occur at maximum Vin.
Open-core inductors have a soft saturation characteristic and they can usually handle higher inductor currents versus a comparable shielded inductor.
A more conservative approach is to select the inductor current rating just for the maximum switch current of the corresponding converter. It must be considered, that the core material from inductor to inductor differs and will have an impact on the efficiency especially at high switching frequencies.
The step-down converter has internal loop compensation. The internal loop compensation is designed to work with an output filter corner frequency calculated as follows:
This leads to the fact the selection of external L-C filter has to be coped with the above equation. As a general rule the product of L × COUT should be constant while selecting smaller inductor or increasing output capacitor value.
Refer to Table 3 and the typical applications for possible inductors.
INDUCTOR TYPE | INDUCTOR VALUE | SUPPLIER |
---|---|---|
BRC1608 | 1.5 µH | Taiyo Yuden |
MLP2012 | 2.2 µH | TDK |
MIPSA2520 | 2.2 µH | FDK |
GLCR1608T1R5M-HC | 1.5 µH | TDK |
LQM21P | 2.2 µH | Murata |
The advanced Fast Response voltage mode control scheme of the step-down converter allows the use of small ceramic capacitors with a typical value of 10 µF, without having large output voltage under and overshoots during heavy load transients. Ceramic capacitors having low ESR values result in lowest output voltage ripple and are therefore recommended. For an inductor value of 1.5 µH or 2.2 µH, an output capacitor with 10 µF can be used. See the recommended components.
If ceramic output capacitors are used, the capacitor RMS ripple current rating will always meet the application requirements. Just for completeness the RMS ripple current is calculated as:
At nominal load currents, the inductive converters operate in PWM mode and the overall output voltage ripple is the sum of the voltage spike caused by the output capacitor ESR plus the voltage ripple caused by charging and discharging the output capacitor:
Where the highest output voltage ripple occurs at the highest input voltage Vin.
At light load currents, the converter operates in Power Save Mode and the output voltage ripple is dependent on the output capacitor value. The output voltage ripple is set by the internal comparator delay and the external capacitor. The typical output voltage ripple is less than 1% of the nominal output voltage.
Because of the nature of the buck converter having a pulsating input current, a low ESR input capacitor is required for best input voltage filtering and minimizing the interference with other circuits caused by high input voltage spikes. The converters need a ceramic input capacitor of 10 μF. The input capacitor can be increased without any limit for better input voltage filtering.
TYPE | VALUE | VOLTAGE RATING | SIZE | SUPPLIER | MATERIAL |
---|---|---|---|---|---|
GRM155R60G475ME47D | 4.7 µF | 4 V | 0402 | Murata | Ceramic X5R |
GRM155R60J225ME15D | 2.2 µF | 6.3 V | 0402 | Murata | Ceramic X5R |
GRM185R60J225 | 2.2 µF | 6.3 V | 0603 | Murata | Ceramic X5R |
GRM188R60J475K | 4.7 µF | 6.3 V | 0603 | Murata | Ceramic X5R |
GRM188R60J106ME47D | 10 µF | 6.3 V | 0603 | Murata | Ceramic X5R |
See Design Requirements, Detailed Design Procedure, and Application Curve.