JAJSLW7B December 2020 – September 2023 TPS6593-Q1
PRODUCTION DATA
The LDOVINT voltage regulator is dedicated to supply the digital and analog functions of the TPS6593-Q1 device, which are not required to be always-on and can be turned-off when the device is in low power states. The LDOVINT voltage regulator is automatically turned on and off as needed if LP_STANDBY_SEL = '1'. The automatic control optimizes the overall current consumption when the device is in low power LP_STANDBY state.
The LDOVINT voltage regulator is dedicated for internal use only, and cannot be used to support external loads. An output filtering capacitor must be connected at the VOUT_LDOVINT pin. Do not connect any other components or external loads to this VOUT_LDOVINT pin.