Added note about unmasking the UV/OV right before the release of the
nRSTOUT resp. nRSTOUT_SoC pins.
Go
Added note which explains the required voltage accuracy for external
supply rails (including VCCA input supply) that are monitored by the TPS6594-Q1
in order to pass the ABIST
Go
Added explanation on how to use Voltage Monitors of unused BUCK and
LDO regulators
Go
Corrected Watchdog Reference Answer Calculation figure
Go
Added note which explains necessary system-software steps for using
RUNTIME_BIST
Go
Changed all instances of legacy terminology into "controller" and
"target", also in all sub-sections
Go
For I2C, changed all instances of legacy terminology into
"controller" and "target". For SPI, changed all instances of legacy terminology
into "controller" and "peripheral". For the CRC, changed all instances of legacy
terminology into "CRC on received data (R_CRC)", and "CRC on transmitted data"
(T_CRC). These changes also applies to all sub-sections.
Go
Corrected figure on Calculation of 8-Bit Controller
CRC (R_CRC) Output, corrected figure on Calculation of 8-Bit
Target CRC (T_CRC) Input
Go
Added note about missing R_CRC after am I2C write
Go
Added note which describes a device erratum related to
COMM_FRM_ERR_INT bit
Go
Added note which explains the I2C addresses for each
register map page on the I2C bus. Added note which explains how each
register map page is addressed when using SPI.
Go
Added note about writing to RESERVED bits causing a Register Map CRC
error
Go