4 Revision History
Changes from Revision D (June 2019) to Revision E (August 2021)
- 文書全体にわたって表、図、相互参照の採番方法を更新Go
- 文書全体で、SPI に言及している場合、従来の用語をコントローラ / ペリフェラルに変更Go
- 「
Section 1
」一覧を更新Go
- 「
Section 2
」セクションを更新Go
Changes from Revision C (August 2016) to Revision D (June 2019)
- 「製品情報」表に NFBGA パッケージを追加Go
- Added NFBGA package to the
Section 6
sectionGo
- Added NFBGA package to the
Section 7.4
tableGo
Changes from Revision B (May 2016) to Revision C (August 2016)
- Added the HRESET I/O voltage parameter to the Absolute Maximum Ratings tableGo
- Changed the value for the HBM from ±2000 to ±1500 in the ESD Ratings tableGo
- Changed the maximum values for the ILDO_3V3 (50 to 70 mA) and ILDO_3V3EX (10 to 30 mA) current parameters in the Power Supply Requirements and Characteristics
Go
- Updated the GPIO_RPU parameter to show values for DEBUG_CTL1/2
separately in the Input/Output (I/O) Characteristics
tableGo
- Added parameters for HRESET in the Input/Output (I/O)
Characteristics tableGo
Changes from Revision A (June 2015) to Revision B (May 2016)
- 編集上の修正により誤字を訂正し用語の整合性を向上Go
Changes from Revision * (March 2015) to Revision A (June 2015)