JAJSM29A april 2023 – july 2023 TPS7A96
PRODUCTION DATA
Wide bandwidth linear regulators suffer from an undesirable excessive overshooting of the output voltage during restart events that occur when the CNR/SS and COUT capacitors are not fully discharged. In this device, and as shown in Figure 8-1, this undesirable behavior is mitigated by implementing low hysteresis circuitry consisting of two ORed comparators to detect when the input voltage is either 20 mV (typical) lower than the VNR/SS reference voltage or 300 mV (typical) lower than VOUT.
When the device is operating in dropout, transient events (such as an input voltage brownout, heavy load transient, or short-circuit event) can force the device in a reversed bias condition where the input voltage is either 20 mV (typical) lower than the VNR/SS reference voltage or 300 mV (typical) lower than VOUT. The output overshoot prevention circuit can be triggered, as shown in Figure 8-2, thus forcing the device to shutdown and restart, thereby preventing output voltage overshoot. If the device is still operating in dropout and the error condition that triggered this circuit is still present, an additional restart can occur until these conditions are removed or the device is no longer in dropout. The restart always occurs from a discharged state and always has the same characteristics as the initial LDO power-up, so the start-up time, VOUT ramp rate, and VOUT monotonicity are all predictable.
Figure 8-3 and Figure 8-4 show examples of a soft brownout and a brownout event, respectively.
The brownout overshoot is present with higher VIN slew rates. A 1-V/μs slew rate was used in Figure 8-5.
The overshoot prevention circuit is implemented to provide a predictable start-up and shutdown of the device without output overshoot if the EN_UV external UVLO is not used as described in this section. This circuit can be prevented from triggering by: