JAJSSS6B January 2024 – June 2024 TPS7H3014-SP
PRODUCTION DATA
The UP and DOWN pins are the inputs that initiate a sequence up or down. Both pins incorporate an accurate comparator with a threshold voltage of VTH_UP = 599mV (for UP) and VTH_DOWN = 498mV (for DOWN) with an accuracy of ±3% for both inputs.
A fixed hysteresis of 100mV is incorporated in both comparators for noise stability. The edges on these pins are used to initiate the command as:
The UP voltage is also used in the state machine as a latch method to prevent oscillations during a FAULT. In order to move away from the Fault state, the UP voltage has to be logic low. As UP is a comparator with 100mV of hysteresis, depending on whether the VUP have been previously above the VTH_UP, the logic low level is:
These inputs can be driven externally by a house-keeping controller or via a resistive divider connected to a voltage source.
As these inputs are edge sensitive, is important to have a stable input voltage (UVLORISE < VIN < 14V) for at least 2.8ms (tStart_up_delay) before sending the sequence up command. This is due to internal time constants in the device. During sequence down, it's important to maintain a stable input voltage until the SEQ_DONE flag is set low to allow all rails to be properly sequenced down.
As both the UP and DOWN pins have accurate undervoltage comparators, the user can program the voltage at which the system will automatically start the sequence up and down when monitoring a main power rail (VMAIN) via a resistive divider. However, in this case it is important to make sure the rising and falling edge are sent when VIN is stable, as mentioned before. A capacitor can be added from UP to GND to delay the signal when the slew rate at VMAIN is fast.
Usually the designer knows the voltages at which it's desired to start the sequence up (referred to as VUP_IDEAL) and down (referred to as VDOWN_IDEAL). With that information we can calculate the resistive divider values using Equation 19 and Equation 20. Usually the top resistor is fixed to a 10kΩ value.
where:
Once the designer knows the actual (real) resistive divider values, Equation 21 and Equation 22 can be used to calculate the sequence up and down nominal voltages as:
If desired, to select the capacitance (CDELAY) for the UP pin we can use Equation 23.
where: