SLUSBU2A September 2014 – February 2016 TPS92661-Q1
PRODUCTION DATA.
The TPS92661 requires a 5-V supply to power the charge pump, internal logic and references. This rail generates a 3.3-V supply which can be used for the digital communications as outlined in the Internal Regulator section. The TPS92661 device is not compatible with logic levels lower then 3.3 V or greater than 5 V. A separate, high-power supply drives the LED string, as discussed in the LED Fault Detection and Protection section.
The VCC pin is the output node of the on-board 3.3-V LDO. The VCC pin also acts as the positive voltage rail for the device digital I/Os. If the TPS92661 device is used with a microcontroller with 3.3-V I/Os, then place an output capacitor with a value of at least 0.1 µF at the pin for the internal LDO. Due to the internal linear regulator, an external 3.3-V supply is not required.
If the TPS92661 device is used with 5-V microcontrollers, then the VCC pin MUST be tied to the 5-V VIN pin. This connection overrides the internal LDO and allows the digital I/Os to signal at 5 V rather than 3.3 V.
In the rare case that the digital signaling exists at a voltage greater than 3.6 V, but less than 4.5 V, then the VCC pin should be connected to the same voltage as the MCU I/O voltage.
When VIN is greater than VIN-UVT , all bypass switches are initially on (LEDs off) and the LEDs remain off until the device is programmed with the corresponding LED and ENABLE registers. After the registers are programmed, the TPS92661 device modulates the LEDs using the divided-down CLK input as the PWM clock. VIN must be greater than VIN-UVT prior to sourcing current through the LED string in order to ensure a controlled start-up.
The EN input acts as an active-low reset signal for the TPS92661 device. If EN = 0, the TPS92661 device resets to the same state as if a power cycle had occurred. All registers are reset to default values and all of the bypass switches are turned on (LEDs off). Once the device emerges from the reset state by setting EN high, the registers must be programmed in order for the device to begin normal operation.
Power consumption increases with increased clock frequency, with VIN voltage and with temperature. It is always best to select the lowest VIN and clock frequency the system can tolerate. Guidelines for power drawn by the device from VIN are provided in the Typical Characteristics section.
Figure 38 outlines the steps required to begin communication with a TPS92661 and enable the LEDs. Register Read and Write code examples are shown in the Programming section.