JAJSJQ7A September 2020 – December 2020 TPSM41625
PRODUCTION DATA
The output voltage of the TPSM41625 is externally adjustable by first setting the reference voltage, VREF, using the VSEL pin and then, if needed, setting the output voltage adjust resistor RADJ. For this application, VREF is the same as the output voltage, so RADJ is not needed and RS+ should be connected to the output rail, near the load.
To set the output voltage to 0.95 V, select VREF of 0.95 V by connecting a 78.7-kΩ resistor between VSEL pin and AGND and connect RS+ pin to the output voltage rail. VSEL resistor values for setting VREF can be found in Table 7-1.