JAJSN49 January 2022 TPSM5D1806E
PRODUCTION DATA
When operating the TPSM5D1806E as a dual output device, the two output voltages (VOUT1 and VOUT2) are set using resistor dividers between the output voltages and AGND with the mid-point of the resistor divider connecting to the corresponding feedback pin (FB1 and FB2). See Figure 7-4.
Select a bottom feedback resistor of 10 kΩ and calculate the value for the top feedback resistor (RFBT) using the following equation. Use divider resistors with 1% tolerance or better and with a temperature coefficient of 100 ppm or lower.
When connecting the two outputs of the TPSM5D1806E for current sharing, the output voltage is set using only a single feedback divider connected to FB1. The FB pin of the second channel, FB2, must be left floating as shown in Figure 7-2. Use Equation 1 to calculate the RFBT.