JAJSKD0 December 2023 TRF1305B2
PRODUCTION DATA
Figure 7-1 shows a functional diagram of the output common-mode control. Internally the VOCM pin sees an LDO output voltage that is equal to VS– + 2.5 V connected through a 2.5‑kΩ resistor.
Floating the VOCM pin is allowed. The output common-mode voltage at the output pins, OUTPx and OUTMx, defaults to the LDO output voltage of VS– + 2.5 V when VOCM pin is floated. Floating the VOCM pin results in a VOCM voltage equal to midsupply when VS = 5 V. If the VOCM pin is driven, then drive the pin from a low-impedance source. Limit the value of ROCM to less than 25 Ω for accurate reflection of the forced VOCM voltage at the device outputs.