The VDD pin must have de-coupling capacitors places as closely to the device as possible. Typically recommended capacitors are a 0.1 µF and 1 µF capacitor.
If FM support is not needed connect GNDA to system GND along with the GND connections with the shortest connections possible.
RING2 and SLEEVE should be routed on the same layer as the audio jack for best performance with less than 50 mΩ to the audio jack pins. These two pins should have priority in layout over other pins. It is recommended to not use vias on these traces and pair the device with an audio jack that facilitates this type of layout.
The RING2_SENSE and SLEEVE_SENSE pins are kelvin connections to the audio jack and should be shorted to RING2 and SLEEVE as close to the audio jack as possible. If there are 0 Ω resistors between the SLEEVE/RING2 pins and the jack, connect the SENSE lines to the jack sleeve and ring2 contacts. If a microphone is connected one of the SENSE lines will carry the microphone signal and the MICBIAS supply. It is recommended that these traces not have more than 1 Ω impedance to the jack.
Route the I2C and digital signals away from the audio signals to prevent coupling onto the audio lines.