SCDS357A July 2014 – December 2014 TS5A3166-Q1
PRODUCTION DATA.
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
SPST analog switch is a basic component that could be used in any electrical system design. The following are some basic applications that utilize the TS5A3166, more detailed applications may be found in the Typical Application section.
Place a switch in series with the input of the op amp. Since the op amp input impedance is very large, a switch on ron(1) is irrelevant.
By choosing values of R1 and R2, such that Rx >> ron(x), ron of TS5A3166 can be ignored. The gain of op amp can be calculated as follow: