JAJSK22 June 2021 TUSB217A
PRODUCTION DATA
The purpose of the TUSB217A is to re-store the signal integrity of a USB High-speed channel up to the USB connector. The loss in signal quality stems from reduced channel bandwidth due to high loss PCB trace and other components that contribute a capacitive load. This can cause the channel to fail the USB near end eye mask. Proper use of the TUSB217A can help to pass this eye mask.
A secondary purpose is to use the CD pin of the TUSB217A to control other blocks on the customer platform, if so desired.