Waveform 1 in Figure 6-6 is for an output with internal such that the output is high, except
when OE is high (see Figure 6-3). Waveform 2 in Figure 6-6 is for an output with conditions such that the output is low, except
when OE is high.
All input pulses are
supplied by generators having the following characteristics: PRR ≤ 10MHz, ZO = 50Ω, dv/dt ≥ 1V/ns.
The outputs are measured
one at a time, with one transition per measurement.