Figure 9-2 depicts the inputs and outputs to this device
that have negative clamping diodes.
CAUTION: Voltages beyond the values
specified in the Absoulte Maximum Ratings table can
cause damage to the device. The input
negative-voltage and output voltage ratings may be
exceeded if the input and output clamp-current
ratings are observed.
Figure 9-2 Electrical Placement of
Clamping Diodes for Each Input and Output