JAJSOL5B april 2023 – august 2023 UCC27301A-Q1
ADVANCE INFORMATION
デバイスごとのパッケージ図は、PDF版データシートをご参照ください。
Generally, the switching speed of the power switch during turnon and turnoff should be as fast as possible in order to minimize switching power losses. The gate driver device must be able to provide the required peak current for achieving the targeted switching speeds with the targeted power MOSFET. The system requirement for the switching speed is typically described in terms of the slew rate of the drain-to-source voltage of the power MOSFET (such as dVDS/dt). For example, the system requirement might state that a SPP20N60C3 power MOSFET must be turned-on with a dVDS/dt of 20 V/ns or higher with a DC bus voltage of 400 V in a continuous-conduction-mode (CCM) boost PFC-converter application. This type of application is an inductive hard-switching application and reducing switching power losses is critical. This requirement means that the entire drain-to-source voltage swing during power MOSFET turnon event (from 400 V in the OFF state to VDS(on) in on state) must be completed in approximately 20 ns or less. When the drain-to-source voltage swing occurs, the Miller charge of the power MOSFET (QGD parameter in the SPP20N60C3 data sheet is 33 nC typical) is supplied by the peak current of gate driver. According to power MOSFET inductive switching mechanism, the gate-to-source voltage of the power MOSFET at this time is the Miller plateau voltage, which is typically a few volts higher than the threshold voltage of the power MOSFET, VGS(TH).
To achieve the targeted dVDS/dt, the
gate driver must be capable of providing the
QGD charge in 20 ns or less. In other
words a peak current of 1.65 A (= 33 nC / 20 ns)
or higher must be provided by the gate driver. The
UCC27301A-Q1 gate driver is
capable of providing 3.7-A peak sourcing current
which clearly exceeds the design requirement and
has the capability to meet the switching speed
needed. The 2.4× overdrive capability provides an
extra margin against part-to-part variations in
the QGD parameter of the power MOSFET
along with additional flexibility to insert
external gate resistors and fine tune the
switching speed for efficiency versus EMI
optimizations. However, in practical designs the
parasitic trace inductance in the gate drive
circuit of the PCB will have a definitive role to
play on the power MOSFET switching speed. The
effect of this trace inductance is to limit the
dI/dt of the output current pulse of the gate
driver. In order to illustrate this, consider
output current pulse waveform from the gate driver
to be approximated to a triangular profile, where
the area under the triangle
(½ × IPEAK ×
time) would equal the total gate charge of the
power MOSFET (QG parameter in
SPP20N60C3 power MOSFET datasheet = 87 nC
typical). If the parasitic trace inductance limits
the dI/dt then a situation may occur in which the
full peak current capability of the gate driver is
not fully achieved in the time required to deliver
the QG required for the power MOSFET
switching. In other words the time parameter in
the equation would dominate and the
IPEAK value of the current pulse would
be much less than the true peak current capability
of the device, while the required QG is
still delivered. Because of this, the desired
switching speed may not be realized, even when
theoretical calculations indicate the gate driver
is capable of achieving the targeted switching
speed. Thus, placing the gate driver device very
close to the power MOSFET and designing a tight
gate drive-loop with minimal PCB trace inductance
is important to realize the full peak-current
capability of the gate driver.