JAJSF47A April 2018 – May 2018 UCC28742
PRODUCTION DATA.
The FB pin connects to the emitter of an analog optocoupler output transistor which usually has the collector connected to VDD. The current supplied to FB by the optocoupler is reduced internally by a factor of 2.5 and the resulting current is applied to an internal 480-kΩ resistor to generate the control law voltage (VCL). This VCL directly determines the converter switching frequency and peak primary current required for regulation per the control-law for any given line and load condition.
Typical circuit connection between FB and optocoupler along with typical values of resistors and capacitors should be made as shown in Figure 9. The resistors and capacitors in the connections help to stabilize operation during control mode transition.