DLPU041G April 2016 – July 2024 DLPC230-Q1 , DLPC230S-Q1
This command is used to reset the DLPC230-Q1. The proper byte signature must be transmitted to initiate the reset in order to prevent unintended system resets.
When the command is received, the DLPC230-Q1 will perform a full reset except for the main PLL. This will not reset the DMD or the TPS99000-Q1. In order to reset the entire chipset, the external PROJ_ON signal should be used.
Write Parameters
BYTE | BITS | DESCRIPTION |
---|---|---|
1 | 7:0 | Signature Byte 1 0xAA |
2 | 7:0 | Signature Byte 2 0xBB |
3 | 7:0 | Signature Byte 3 0xCC |
4 | 7:0 | Signature Byte 4 0xDD |