DLPU041G April 2016 – July 2024 DLPC230-Q1 , DLPC230S-Q1
External Video Checksum Settings command is used to specify the desired window of video pixels. This command can also be read to confirm the actual checksum of the current video data.
Figure 6-5 demonstrates the checksum region configuration.
Settings should only be modified while the test is disabled. If changes need to be made to the settings, the test should be disabled and then re-enabled after settings have been applied.