DLPU041G April 2016 – July 2024 DLPC230-Q1 , DLPC230S-Q1
This command is used to read the embedded software operating mode. Refer to Section 4.1 for descriptions of operating modes.
The Short Status command can also be used to read the current operating mode. Using the Short Status is faster than using this command since the Short Status can be read in one transaction.
Command Parameters
No command parameters.
Return Parameters
BYTE | BITS | DESCRIPTION |
---|---|---|
1 | 7:2 | Reserved |
1:0 | Operating Mode 0x0: Standby 0x1: Display 0x2: Calibration 0x3: Reserved |