DLPU041G April 2016 – July 2024 DLPC230-Q1 , DLPC230S-Q1
This command directs the boot application to erase the entire contents of the flash device.
The Request in Progress bit of the Short Status will be set at the start of the flash erase process and will be cleared when the erase process is complete.
The error bits in the Short Status can be used to determine whether an error occurred during the erase process.
More information on flash programming can be found in Section 5.3.3.
Write Parameters
BYTE | BITS | DESCRIPTION |
---|---|---|
1 | 7:0 | Signature Byte 1 0xAA |
2 | 7:0 | Signature Byte 2 0xBB |
3 | 7:0 | Signature Byte 3 0xCC |
4 | 7:0 | Signature Byte 4 0xDD |