DLPU041G April 2016 – July 2024 DLPC230-Q1 , DLPC230S-Q1
This test monitors system voltage levels each frame using TPS99000-Q1 ADC measurements. The following voltages are monitored:
If any of these voltages are measured outside of a specified maximum and minimum value, the test will take action. The monitor ranges are specified in the flash header file provided along with the flash binary file. The true voltage operating ranges are specified in the DLPC230-Q1 Data Sheet and TPS99000-Q1 Data Sheet. The monitor ranges used for this test are set wider than the true voltage operating ranges to account for measurement tolerances.