DLPU048E August 2016 – July 2024
If the Command Error or Communication Error bits are set in the error, then the information bits will provide the following information.
BITS | DESCRIPTION |
---|---|
15:8 | Command tag Tag of the command that received the error. |
7:0 | Command Op-Code Op-code of the command that received the error. |