DLPU048E August 2016 – July 2024
This command is used to read back the current illumination pulse error information while operating in discontinuous mode.
Command Parameters
No command parameters.
Return Parameters
BYTE | BITS | DESCRIPTION |
---|---|---|
1 | 7:3 | Reserved |
2 | Pulse Width Error Flag Indicates that the SEN signal was held low longer than the maximum allowable time for a single pulse and was therefore forced high. This typically indicates that a light pulse was unable to achieve the desired photo feedback level within the allocated pulse time. 0x0: No error 0x1: Error | |
1 | Pulse Count Error Flag Indicates that too few pulses were generated within a bit slice. 0x0: No error 0x1: Error | |
0 | No Compare Error Flag Indicates that COMPOUT never went low within a bit slice. 0x0: No error 0x1: Error |