DLPU048E August 2016 – July 2024
This command is used to execute a batch command set that is stored in flash. More information of batch command sets can be found in Section 5.2.
Write Parameters
BYTE | BITS | DESCRIPTION |
---|---|---|
1 | 7:0 | Batch index Index of the batch command set stored in flash (0-based). |